AnsweredAssumed Answered

AD-FMCOMMS1-EBZ  No OS Ref Design - ADC Function Parameters?

Question asked by DrTom on Mar 8, 2013
Latest reply on Mar 8, 2013 by rejeesh

Within the reference design there is a adc_test() function that test the board by forcing the ADC to output a specific value or pattern. There is a write to the ADC(?)  at the beginning of adc_test()

Xil_Out32(XPAR_AXI_ADC_2C_0_BASEADDR + 0x2C, 0);

and a similar write at the end of the test

Xil_Out32(XPAR_AXI_ADC_2C_0_BASEADDR + 0x2C,0x2);

 

These are not commented nor can I find what/where the 0x2C register is. The XPAR_AXI_ADC_2C_0_BASEADDR is address of the axi interfce to the adc channel 0 I assume.

Can anyone help?

Thanks...Tom

Outcomes