AnsweredAssumed Answered

How to disable a workaround

Question asked by Haje on Mar 7, 2013
Latest reply on Mar 8, 2013 by Haje

Hi

I'm using ADSP-21371. When I look at the statistical profiler, I see that almost 8% of the time is spent @90101, which seems to come from the workaround for anomaly 09000011.

I believe that this anomaly does not apply in my case, as I do not execute any code from external memory, I only have data acces to external memory.

Thus, I tried to disable this workaround but have not succeded. When I add the line '-no-workaround 09000011' in the compiler options, I get following error:

 

cc3141: {D} error: Unknown work-around name `09000011'

 

Accordingd to SHARC-2136X-anomaly.xml, this anomaly workaround is assembler-only.

 

How can I disable it?

 

Thank you in advance

Hans

 

p.s. I'm using VisualDSP++ 5.0 Update 10.1.

Outcomes