AnsweredAssumed Answered

The output voltage (Voh) of the ADuC7023

Question asked by Whitetail on Mar 7, 2013
Latest reply on Apr 3, 2013 by wallman16

Could you please let me know regarding the Logic Output Voltage Level of the ADuC7023.

What level is the output voltage when it's used at IOVdd = 3.5V? Is Voh(min)= 2.4V and Vol(max) =  .

The voltage of Typical logic device input is Vdd x 0.7V. Thus Vih(min) will be 2.45V.

Do we need to use any interface devices?

Do you have any data  with regards to IOVdd of the ADuC7023?

Outcomes