AnsweredAssumed Answered

Can I use Qt Creator as GDB front-end?

Question asked by skstrobel on Mar 5, 2013
Latest reply on Mar 6, 2013 by Aaronwu

I have a Qt application that builds and runs fine on Windows, but crashes when run on my Blackfin target.  I can load it into gdbserver on the target and could probably connect to that and debug using the command line gdb on my host, but that isn't very user-friendly.  I would like to use Qt Creator as a front end for gdb, but the only options I see in the debug menu are for x86 and Arm, neither of which work well with my Blackfin target.  The version of Qt Creator I have installed on my Ubuntu 10.04 host is V2.5, which is based on Qt 4.8.1.  Is there another version of Qt Creator which works well?  I could run it on either Ubuntu or Windows.  Thanks.

 

Steve

Outcomes