AnsweredAssumed Answered

ADV7511 usage to output interlacing video modes

Question asked by NLaeaeper Employee on Mar 4, 2013
Latest reply on Mar 4, 2013 by GuenterL

Is it right that ADV7511 cannot be used to output interlacing video modes like HDTV 1080i if color space RGB is needed, because there is no Input ID available that combines RGB and
input embedded syncs (the field is to set in
the output embedded syncs, but ADV7511 does not accept the field information (even or odd) on a pin with separate syncs. I intend to
use Input ID = 0 (R0x15
[3:0])

 

Is there a way that I do not see?

Outcomes