AnsweredAssumed Answered

Error in adc library code?

Question asked by J-dawg on Feb 27, 2013
Latest reply on Feb 27, 2013 by J-dawg

Hello ADI

 

Im sitting with the EVAL-ADUCM360MKZ board and are testing a lot of different settings with the ADC.

Im using the library code found at: ftp://ftp.analog.com/pub/MicroConverter/ADuCM360V1.0/Code/common/

Latest update seems to be: 09/26/2012 12:00.

In this code i was unable to set the averaging factor AF. I use the function adcflt();

In the code it AND's all the input parameters with different bits which is fine with all except the AF. Here it ANDs the input parameter (decimal 0-14) with 0xF00. Which will always be 0 due to the fact that AF never will exceed 0xE. Therefore you need to bitshift the AF value by 8 and the code works. My question is:

Am i using the latest update of the code in adclib.c?

Outcomes