AnsweredAssumed Answered

ADV7343 CLKIN level @VDDIO=1.8V

Question asked by YuichiMASUDA on Feb 27, 2013
Latest reply on Feb 27, 2013 by YuichiMASUDA

Dear

 

In case of using VDDIO= 1.8V, do CLKIN_A and CLKIN_B Input level obey to following condition?

 

DIGITAL INPUT/OUTPUT SPECIFICATIONS—1.8 V (quoted from ADV7343 datasheet Rev.D, page.8)

When VDD_IO is set to 1.8 V, all the digital video inputs and control inputs, such as I2C, HS, and VS, should use 1.8 V levels.

 

According to this sentence, the below pin are targeted.

C0-7/S0-7/Y0-7ALSB/SFLS_VSYNC/S_HSYNCP_VSYNC/P_HSYNC/P_BLANKSDA/SCL


Outcomes