AnsweredAssumed Answered

Having problem with RX62N_library.lib

Question asked by notarboca on Feb 25, 2013
Latest reply on Feb 26, 2013 by notarboca

Greetings, I seem to have a problem when building the project for the first time:

 

Phase: OptLinker, File: OptLinker, dependency scan error

DL201 (E) The specified file does not exist 'C:\WorkSpace\ADIEvalBoard\ADIEvalBoard\RPDL\RX62N_library.lib'

Building - ADIEvalBoard - Debug

 

Phase RX C/C++ Library Generator starting

Phase RX C/C++ Library Generator finished

 

Phase RX C/C++ Compiler starting

C:\WorkSpace\ADIEvalBoard\ADIEvalBoard\dbsct.c

C:\WorkSpace\ADIEvalBoard\ADIEvalBoard\sbrk.c

C:\WorkSpace\ADIEvalBoard\ADIEvalBoard\resetprg.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_WDT.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_ADC_10.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_ADC_12.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_BSC.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_CMT.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_DMAC.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_EXDMAC.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_IIC.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_INTC.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_MTU2.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_not_RPDL.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_INTC.c(419) :  C5167 (W) Argument of type "uint32_t" is incompatible with parameter of type "void *"

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_POE.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_RTC.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_SCI.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_SPI.c

C:\WorkSpace\ADIEvalBoard\RPDL\Interrupt_TMR.c

Phase RX C/C++ Compiler finished

 

Phase OptLinker starting

License expires in 59 days

L3300 (F) Cannot open file : "C:\WorkSpace\ADIEvalBoard\ADIEvalBoard\RPDL\RX62N_library.lib"

Optimizing Linkage Editor Abort

Build Stopped - Fatal Error

1 Error, 1 Warning

 

Can anyone give me any suggestions; I thought I followed the ADI instructions as I should have.

Outcomes