AnsweredAssumed Answered

High ÷N value Programmable Divider...?

Question asked by YSVenu on Feb 22, 2013
Latest reply on May 1, 2013 by icollins

Hi Engineer Zone,

 

My application requires a Programmable Divider. The system input (square wave) frequency varies from 1MHz to 30MHz. I should be able to divide the incoming frequency to 500Hz.

So, max 30MHz/500Hz will be a divide count of 60,000.

 

Can I use any of ADI IC's to do such a large scale division...? I read that this was possible with a dual modulus prescaler.

 

Advance Thanks,

YSVenu

Outcomes