AnsweredAssumed Answered

re: similarities between 21489 and 21469

Question asked by Nav@AT on Feb 22, 2013
Latest reply on Mar 14, 2013 by Harshit.Gaharwar

Hi,

 

I'm working on a 21489 processor with code that was written on a 21469 processor. There are a few files in the project that are related to 21469 such as cdef21469, SRU21469 and ADDS_Ezkit_21469.

 

To run the code without any build errors I changed 21469 to 21489 in two places -

     1. Project Options -> Target Processor

     2. I replaced the "ARCHITECTURE" in the ldf file to 21489 (open with source window)

 

Are these 2 steps sufficient? Should I replace everything I see in the code that reads 21469 to 21489?

 

Regards,

Naveen

Outcomes