vito

PRIM_MODE and VID_STD for UXGA60 (ADV7611, ADV7612, ADV7619)

Discussion created by vito on Feb 19, 2013
Latest reply on Jan 8, 2014 by Austride

Hi,

 

Setting HDMI input type has only to do with Free Running;

additionally when parameters are auto-buffered - the HDMI receiver

will output free run timing of exactly same parameters as previously received.

Therefore in many scripts we set part to HDMI-COMP 525P.

 

This are settings to enable UXGA60 Free-Run without free running:

 

     UXGA60:

     PRIM_MODE = HMDI-GR.

     VID_STD = 010110     UXGA 1600x1200 @60

 

     UXGA60-with reduced blanking:

     PRIM_MODE = HMDI-GR.

     VID_STD = 010111 UXGAR 1600x1200 @60

 

Above settings will be added to the next revision of hardware manual of ADV7611, ADV7612, ADV7619

 

Rgds,

vito

Outcomes