AnsweredAssumed Answered

ADP223ACPZ output voltage adjustment

Question asked by DarrenH on Feb 18, 2013
Latest reply on Feb 18, 2013 by DarrenH

I am using a ADP223 device on one of my prototype cards and I have a question about setting the output voltage on both VOUT1 and VOUT2.

With VIN at +3.3V I want to have +0.5V on VOUT1 and VOUT2, do I have just a 0R resistor connected between the ADJ pin and the VOUT pin on both channels to give me the required +0.5V output? The EN1 and EN2 pins are connected to VIN for auto startup.

 

Darren

Outcomes