AnsweredAssumed Answered

Measuring non-terminated LVDS outputs.

Question asked by ppez on Feb 11, 2013
Latest reply on Feb 21, 2013 by ConalW

If I do not terminate the LVDS (ADN4661) outputs with a 100 ohm resistor, can I still measure one of the outputs using a single-end measurement using the O-scopes 50 or 1 M ohm impedance setting. See attached file. If so, what is the voltage swing?

 

If not, can I still make the same measurement if I add the 100 ohm termination? What is the voltage swing? Thanks.

Attachments

Outcomes