AnsweredAssumed Answered

Can we short output pins MSBOUT and VOUT of AD5932?

Question asked by guru on Feb 8, 2013
Latest reply on Feb 8, 2013 by musach

In my application I will be using either sine wave or square wave output at a time. On my board there is no space to put analog mux to select one of two output. Can I short the two output pins of IC (MSBOUT and VOUT)

On page 16 in datasheet its mentioned that we can disable DAC by setting  DAC Enable pin to 0 and we can disable MSBOUT by MSBOUTEN=0. So if I want sine wave output I will disable MSBOUTEN and if I want square wave output I will disable DAC Enable bit and enable only MSBOUTEN.

 

Will this work?

Outcomes