AnsweredAssumed Answered

ADAU1701 Loading Procedure

Question asked by Raydon on Feb 6, 2013
Latest reply on Feb 6, 2013 by BrettG

Hi all,

 

I am working on removing the EEPROM (cost reduction) from a my project that is currently working in self-boot mode.  I was hopeful that I could write the Program data and then the Parameter data in continuous streams (i.e., write all 5120 Program bytes at once) .   I noted in the data sheet that Tables 23 & 25 seem to suggest that Parameter RAM Burst Mode write is limited to 15 bytes and Program RAM Burst Mode write is limited to 18 bytes.  Are Burst Mode data bytes 'length' limited or can I write all data in a single transmission?

 

Thanks,

Ray

Outcomes