AnsweredAssumed Answered

ts201

Question asked by lzping on Feb 6, 2013
Latest reply on Feb 12, 2013 by jeyanthi.jegadeesan

HI!

QUESTION 1:

I use TS201 IRQ0 interrupt, sometimes I find that when using the RTI out of the interrupt, the corresponding PMASK hasn't been cleared,SO the

programs cannot into the interrupt again.

 

QUESTION 2:

I use  link port of two DSP and

Procedures used were used to link two DSP  through the dedicated DMA channels to receive the same data from FPGA, in order to keep the synchronization of the receiving, I AND the two LXACKO signals as FPGA transmit enable signal, but the result is a DSP success, another DSP ONLY received a portion of the data.

 

THANK YOU




Outcomes