AnsweredAssumed Answered

Max. power dissipation of REF195ESZ?

Question asked by aryhanen on Feb 5, 2013
Latest reply on Feb 5, 2013 by VickyW

Hello all!

 

There's no information about the maximum power dissipation of the REF195ESZ in the datasheet. I have an application with the following conditions:

 

REF195ESZ input voltage 13V

Output load 11 mA

 

The power dissipation is (13V-5V)*0,011A = 0,088W. Is this too much?

 

Br,

Antti Ryhänen

Outcomes