AnsweredAssumed Answered

AD5933 Custom Circuits

Question asked by fireexit on Feb 1, 2013
Latest reply on Feb 4, 2013 by musach

Dear Miguel,

 

I am using the AD5933 in a new product design.   The work with the AD5933 evaluation board AD5933EBZ went really well,with some work the system is capable of doing very accurate things.

 

Some questions:

 

I intent to virtually keep all of the circuit in my product and just add in the extra bit of signal conditioning (some EMF protection) plus a socket, would it be possible to get a copy of the original board layout - preferably importable into something easy like DesignSpark?? 

 

If I have to go it alone and start from scratch for the board layout, I notice that there is 2 ADP3303 regulators on the board - do I need the two keeping the refs for the digital and signal conditioning apart.

 

 

Best regards

 

Charlotte

Outcomes