AnsweredAssumed Answered

What is the minimum conversion rate for AD6649?

Question asked by vtrandal on Jan 27, 2013
Latest reply on Jan 27, 2013 by David.Buchanan

Hello,

 

In the data sheet for the AD6649 the minimum conversion rate is stated as 40 MSPS. Maybe the CLK+ and CLK- inputs are AC coupled to block DC. But I would like the AD6649 CLK inputs to work as low as 30 MHz or lower. I tried using an old function generator with a 1 MHz maximum and that results in missing or corrupt data in Visual Analog. Will the AD6649 just not work at speeds lower than 40 MSPS?

 

Thanks!

 

Vincent Randal

Longmont, Colorado

Outcomes