AnsweredAssumed Answered

why readback only in 24.0 format?

Question asked by BerndH on Aug 20, 2009
Latest reply on Jul 29, 2013 by BrettG

Why is it not possible to readback values in 28.0 format? I think this would be very useful!!!

 

For example I would like to monitor the value that is fed to a index selected mux. As far as I can see this input is in 28.0 format. When I use the readback cell I can only select 24.0 format as a maximum. So I always see 0.0000000.

 

A similar problem is monitoring te AUX ADC value. Here I'd like to monitor the value to calculate the divider that is needed to feed a lookuptable which in turn feeds a "sigle slew ext vol". This is to control volume with predefined steps and range using an ext. pot.

 

Regards

Bernd

Outcomes