AnsweredAssumed Answered

Problem in serial communication at 12.58 MHz clock freq

Question asked by smita.patil on Jan 17, 2013
Latest reply on Jan 24, 2013 by MMA

Hi,

 

We Have used ADuC848BSZ62-3(52pin-TQFP) in our project.We have built serial communication between PC & board using UART(at 9600 baud rate).By using technical notes & sample codes,we developed software code for UART module by using timer 2 in baud rate generation mode.We found that it works fine i.e. properly data receive/transmit at clock frequencies of 1.5Mhz & further 3Mhz, 6Mhz( clock frequency is set through PLL) but its not working at 12Mhz clock( CD bits=0) .We are using external crystal of 32.768Khz with 12pf capacitors connected to XTAL 1&2 pins.MCU operating voltage is 5v.We have also checked PLL lock condition. So help me to reslove this issue.

Outcomes