AnsweredAssumed Answered

Video Encoder

Question asked by funk48 Employee on Jan 17, 2013
Latest reply on Jan 18, 2013 by FrankK

Hi,

 

My customer is looking for video encoder which support below signal.

 

Input Data:

    Input data format : 8bit YCbCr EAV/SAV (BT.656)

    Resolution:            640 x 480 (Active)

    Frame Rate:          Progressive 59.940Hz

   Clock Frequency:   50.35MHz

 

I checked the ADV734x and ADV739x data sheet but these device support only 8-bit DDR.

Is there register setting for ADV734x or ADV739x to accept above signal or is there a device to encode such signal?

 

Thanks,

Satoshi

Outcomes