AnsweredAssumed Answered

ADV7183/84 ident code

Question asked by HankZ on Jan 16, 2013
Latest reply on Jan 21, 2013 by DerekBurke

We manufacture a product using either the ADV7183 or ADV7184 and I would like to be able to distinguish between the two models via code.

  

So far, I am aware that the IDENT register (0x11, p. 86 of the above-mentioned manual) can return 0x11 or 0x19 depending on the case.

  

I was wondering whether you could confirm that this is indeed the case, and if possible, explain the possible meanings of the different possible bit permutations for this particular register (as the cells to the right in the table, as pictured below, are empty).

Outcomes