AnsweredAssumed Answered

AD9914 type-o's

Question asked by Halausteve on Jan 16, 2013
Latest reply on Jan 18, 2013 by Halausteve

Please consider the following as possible type errors in the AD9914 Datasheet

 

WHERE:            AD9914 (Rev. A) Page 5, bottom, In Digital Timing Specifications/Test Conditions box:

WHAT IT SAYS: USR0 register, Bit 6=0

Should say??:     CFR1 register, Bit 6=0

 

One more... Page 41, bottom, in Description box:

currently says: PLL lock condition can be read back via Bit 24 in Register 0x00

Should say??: PLL lock condition can be read back via Bit 24 in Register USR0

 

S.

Outcomes