AnsweredAssumed Answered

BF537 STAMP Board and USB-LAN extender problem

Question asked by MLM on Jan 16, 2013
Latest reply on Jan 23, 2013 by Aaronwu

After following the directions "set sw6.4 off, and the modify Linux Kernel Configuration I rebuilt the distribution ADI-2011R1-RC4_45 and installing the USB-LAN board I received the following messages with and without the extender board:

  

U-Boot 2011.09 (ADI-2011R1) (Dec 14 2011 - 13:56:11)

 

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2) (bypass boot)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 125 MHz

RAM:   64 MiB

Flash: 4 MiB

MMC:  

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   bfin_macWarning: failed to set MAC address

 

Hit any key to stop autoboot:  0

*** ERROR: `ethaddr' not set

Wrong Image Format for bootm command

ERROR: can't get kernel image!

bfin>

If I set the switch sw6.4 on, then I can boot normally, but the extender ports (ethernet or USB) do not appear in ifconfig...

 

Any ideas?

 

Best Regards,

Myrick

Outcomes