AnsweredAssumed Answered

BF 537 Frame Capture and save to jpeg APP issue

Question asked by name on Jan 16, 2013
Latest reply on Jan 31, 2013 by rajv

Hello,

 

Please give me an advice regarding a project I'm working on. In BlackfinSDK-3.10  there is FrameCapture1 project that I try to run. The problem is that image comes from the camera distorsioned, you can see in the attached file. You can see the image following these steps:

 

  View -> Debug Windows -> Image Viewer

  Set the Start address to sFrame0

  Pixel Format UYVY (4:2:2)

  Width 864

  Height 525

 

 

 

One more thing, it works only on debug mode. If I press build in release mode, it triggers this error:

Linking...

 

 

[Warning li2060]  The following input section(s) that contain program code

        and/or data have not been placed into the executable for processor 'p0'

        as there are no relevant commands specified in the LDF:

 

 

        .\Release\FrameCapture.doj(sdram0)

        __initsbsz532.doj(bsz_init)

        crtn532y.doj(.gdtl)

        crtn532y.doj(ctorl)

 

 

 

 

[Error li1060]  The following symbols are referenced, but not mapped:

        '_sFrame0' referenced from .\Release\FrameCapture.doj(program)

 

 

Linker finished with 1 error and 1 warning

cc3089: fatal error: Link failed

Tool failed with exit/exception code: 1.

Build was unsuccessful.

 

I use a Panasonic camera which uses PAL format and records at 320X240 pixels, and a Blackfin 537 proccessor.

 

If you need any other details, just replay and I'd be happy to give them to you.

Attachments

Outcomes