AnsweredAssumed Answered

Setting the EBIU Registers

Question asked by spflanze on Jan 11, 2013
Latest reply on Jan 14, 2013 by CraigG

I have seen two ways to set the EBIU registers. One of them is with a custom xml file, and the other is to define and initcode() function in a header. The xml file method does not work when booting from a target board's flash memory. For that the initcode() function must be defined.

 

For a VDK project which file should include the header file containing the initcode() definition?

 

Would the initcode() function in the header file also be executed when the code is downloaded using a JTAG ICE (in my case an ADZS-USB-ICE) instead of loaded from flash?

Outcomes