AnsweredAssumed Answered

AD-FMCOMMS1 2 DAC interfaces?

Question asked by AdrianHolmes on Jan 10, 2013
Latest reply on Jan 10, 2013 by rejeesh

Looking at the UCF and the design in EDK (ML605) there are two interfaces to the DAC. dac0 and dac1. It appears, from the pinout that one dac interface is routed to the FMC LPC connector and one is routed to the FMC HPC connector. Is that correct and does that mean the AD-FMCOMMS FMC board can be connected to either FMC connector on the ML605?

 

Regards,

Adrian

Outcomes