AnsweredAssumed Answered

Crosscore convert dxe to ldr

Question asked by steinp on Jan 9, 2013
Latest reply on Jan 9, 2013 by CraigG

Hello everybody,

 

i would like to convert a dxe to a ldr file and then upload it to the burst flash of the BF-548EZboard.

The dxe file runs in the debug mode.

When creating a ldr file i use the "crosscore blackfin loader" with the following setups:

 

-v proc ADSP-BF548 -si-revision 0.4 -b flash -f hex -width 16 -init myfile.dxe

 

is this for the correct setup for creating a bootable application in burst flash?

 

Can i upload the code into the flash via the flash programmer of the VisualDSP++?

 

Kind regards

Outcomes