AnsweredAssumed Answered

Why  the same code can run in core0 well, but anomaly in core1?

Question asked by kevinxiao on Jan 8, 2013
Latest reply on Jan 31, 2013 by kevinxiao

Hi,

 

I want to run stdio(uart) code in core1 of bf609, I do some things like this:

1. I write stdio code,and debug in core0, it run well, and get print msg form uart ;

2. I  removed the code to core1,and add adi_core_1_enable()  then while(1) in core0;

3. Running core1, uart port getting nothing, progam run remainning at adi_uart_write(); it means run anomaly;

 

Do you know why the same code can run in core0 well, but run anomaly in core1?

The platform is ADZS-BF609-EZ-BRD Version: 1.0; CCES v1.0.1;

 

Thanks

Kevin

Outcomes