ymwlike

ADSP-21369-CCES project to add a set of analog input

Discussion created by ymwlike on Jan 7, 2013
Latest reply on Jan 8, 2013 by ymwlike

hi,

I add a group of analog input ADSP-21369-CCES project, rewritten in accordance with the ADSP-21489-CCES project.

Questions are as follows:
1.Everything is normal in the hardware simulation to work.
2.but Downloaded to the flash, let it run independently, often with some errors.Some modules can not be normal control,for example the mute not the mute and so on,Why?

Modify the file as follows

InitSPORT.c :Like setting with 21489

initAduio.c:ANALOG_IN_ANALOG_OUT 。

app.c:void GetInputData(void) the same with 21489.

app.h :the same with 21489.

 

Regards,

yamit.

Outcomes