AnsweredAssumed Answered

adv7511 - ZC702 - no display on HDMI port

Question asked by anupkini on Jan 7, 2013
Latest reply on Jan 9, 2013 by anupkini

Hi all,

 

I have a ZYNQ ZC702 evaluation board with adv7511 as the HDMI controller.

I followed the guide on http://wiki.analog.com/resources/tools-software/linux-drivers/platforms/zynq to build and setup the environment.

 

I am unable to get an display through the HDMI port, instead the console is displayed through the USB-UART.

 

I get the following message..

-- cut above this line ---

NET: Registered protocol family 17

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

Registering SWP/SWPB emulation handler

drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

Waiting for root device /dev/mmcblk0p2...

mmc0: new high speed SDHC card at address aaaa

mmcblk0: mmc0:aaaa SU08G 7.40 GiB

mmcblk0: p1 p2

EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)

VFS: Mounted root (ext4 filesystem) on device 179:2.

Freeing init memory: 148K

init: Failed to create pty - disabling logging for job

init: Temporary process spawn error: No space left on device

modprobe: FATAL: Could not load /lib/modules/3.5.0-14.3-build2/modules.dep: No such file or directory

 

-- cut above this, they were all a pass --

 

* Starting load fallback graphics devices                               [fail]

 

-- rest all pass ---

 

speech-dispatcher disabled; edit /etc/default/speech-dispatcher

saned disabled; edit /etc/default/saned

Last login: Thu Jan  1 00:00:09 UTC 1970 on tty1

Welcome to Linaro 12.06 (GNU/Linux 3.5.0-14.3-build2 armv7l)

   * Documentation:  https://wiki.linaro.org/

 

376 packages can be updated.

135 updates are security updates.

 

376 packages can be updated.

135 updates are security updates.

 

376 packages can be updated.

135 updates are security updates.

 

  root@linaro-ubuntu-desktop:~#

 

 

Any suggestions on how to fix this ??

Outcomes