AnsweredAssumed Answered

missing .bit files in FMCOMMS ?

Question asked by LouisBe on Dec 28, 2012
Latest reply on Dec 28, 2012 by LouisBe

Hello,

 

I just received my FMCOMMS module. I want to use it on an ML-605 board.

 

The quick start section says :

The HDL Reference Design for each supported Xilinx FPGA board contains a folder called SDK_Workspace which stores the Xilinx SDK project files needed to build the no-OS software and also the .bit files with the HDL design that must be programmed into the FPGA

 

There is no SDK_Workspace folder neither .bit files for the ML-605 in the fpgahdl_xilinx-master\cf_xcomm\sw i downloaded.

 

Am I missing something or not looking/downloaded the correct files ?

 

Do I have to rebuild the .bit file ?

 

Thanks for the feedback,

 

Louis Belanger.

Outcomes