AnsweredAssumed Answered

AD7626 selection between echo and self clocking.

Question asked by haileysDad on Dec 18, 2012
Latest reply on Jan 10, 2013 by jcolao

Hello,

 

We are using the AD7626 in our latest design and would like to support both self-clock and echo-clock just by changing the FPGA load (no hardware jumper to ground on the DCO+ pin).  In the design the AD7626 DCO+/- LVDS pins are tied directly to a pair of pins on the FPGA.  The FPGA pins can be configured as an LVDS input pair or, by changing the FPGA load, the pin connected to the DCO+ pin can be configured as an output tied to logic '0' in the FPGA.  Another twist is I'm using an SRAM-based FPGA that will take several milliseconds to configure during which time the pins tied to the DCO+/- pins are inputs.  They would remain inputs (as an LVDS input pair) if I use echo clock mode.  If I want to use self-clocking mode the FPGA design loaded would set the DCO+ pin as an output tied to logic '0'.  When does the AD7626 "sense" the DCO+ pin connection to decide which mode to use?

 

Thanks

David

Outcomes