AnsweredAssumed Answered

AD9954 PCBZ  evaluation board  setting

Question asked by KYO on Dec 13, 2012
Latest reply on Dec 18, 2012 by sitti

My English is not good , so don't mind.

MCU:SILICON LABS  C8051FX20-TB    晶片:C8051F120

http://www.silabs.com/Support%20Documents/TechnicalDocs/C8051F12x-13x.pdf

evaluation board:ANALOG DEVICES AD9954

http://www.analog.com/static/imported-files/data_sheets/AD9954.pdf

 

AD9954 evaluation board:

   only use DUT1

   power:VDD_I/O=3.3V   VCC=DVDD=AVDD=1.8V

   U13:PS0、PS1、OSK、I/O SYNC、PD  are ground

       CLKMODESEL=1.8V,RB_ENABLE don't connect anything

       SCLK、SDIO、FUD、RESET、CS  connect with Port4 of 8051

       SDIO(Logic 1)=2.8V,other Pin(logic 1)為3.3V,I don't know why that happen.

   REF_CLK_DUT1  connect to signal generator(12MHz Square wave  150mVpp  offset:75mV)

   because no Oscillator on board.

 

 

 

 

Code(use C code):

使用:Silicon Laboratories IDE編輯

http://dropcanvas.com/m70cr

 

 

Q1:Why don't I get the data of CFR2 by using SDO?

Q2:No output ?

Q3:Why the logic 1 of SDIO pin is 2.8V

 

Thank you~~

Attachments

Outcomes