AnsweredAssumed Answered

AD524 Input/Output Offset Null Potentiometer Value

Question asked by wilsonjr on Dec 12, 2012
Latest reply on Dec 12, 2012 by harryh

Hello,

I have an AD524 being used in an application that may require input and output offset nulling. The AD524 is being used with a gain of 10. I would like to know what value to start with for the pot for both the input and output offset null. +VS is +14V and -VS is -14V. Here is the diagram from the schematic showing the pot but I can't find any indication of value. Any help would be appreciated. Thanks

 

 

Outcomes