AnsweredAssumed Answered

LwIP on BF537 not working with Marvell switch

Question asked by silenuszhi on Dec 11, 2012
Latest reply on Dec 18, 2012 by silenuszhi
Branched from an earlier discussion

Hi Crag,

     I'm using a bf537 custom board and I connected bf537 mac to marvell 88e6351 switch on port 4,and port 4 is configured as a MII mode.I connected a router to port 1 to make a DHCP server.

 

     And when I use the default project in vdsp++5.0 update 10 ,it will lingers when check if the connection is established.And I comment out these lines in the driver to not let 537 check.

 

     And then it goto the acquire of the IP address.After some time, it will show

 

ip address:

 

     so what i should do next?is there some reg in switch to configure?

Outcomes