AnsweredAssumed Answered

maximum sample rate of the ASRC on ADSP-21489

Question asked by jobe on Dec 10, 2012
Latest reply on Mar 27, 2015 by weiss2496

Hello,

 

i've got a question concerning the ASRC on the ADSP-21489.

 

Where can I find a specification for the maximum sample rate of the ASRC? In the hardware reference (http://www.analog.com/static/imported-files/processor_manuals/ADSP-214xx_hwr_r1-0.pdf), there is just the answer "up to 192kHz" in the part "Features". But maybe it's possible to use it with 200kHz? Or even more?

As there are not always exact clocks, I think, there should be given a tolerance. Can you pleace tell me, where I can find this specification?

 

thanks,

Johannes

Outcomes