AnsweredAssumed Answered

ADV3002 HDMI switch query

Question asked by Cman Employee on Nov 29, 2012
Latest reply on Jan 9, 2013 by daverowe

Hello ADV Experts,

 

Q1:
* Regarding the maximum data rate of a HDMI switch ADV3002. On the website I can see this rated up to 3Gbps

(http://www.analog.com/en/audiovideo-products/analoghdmidvi-interfaces/pr).oducts/index.html

 

But in the datasheet is not clear/specific for beyond :
"Supports 250 Mbps to 2.25 Gbps data rates and beyond", see http://www.analog.com/static/imported-files/data_sheets/ADV3002.pdf .

Require a switch for 300MHz clk rate applications. The datasheet  rev.B table 1 only state a Min of 225Mhz. Please can you advise what's the Typ and the Max ! (as there is no figure given?)

 

Q2:
* is if there's a solution for a HDMI1.4a compliant transmitter up to 3Gbps?

Please, can you advise and also cc to Marcos.OteroGensheimer@barco.com

 

Thanks and regards,

Ching

 

Outcomes