AnsweredAssumed Answered

BF357 LwIP running from flash

Question asked by Dazdranagorn on Nov 9, 2012
Latest reply on Nov 13, 2012 by Dazdranagorn

Hello, I'm trying to start my application based on Caesar_Cipher example.

It works perfectly when I start it as executable(*.dxe)

 

I tried to load it to flash memory, but have failed.

 

In project options I set type “Loader file

Checked in Load submenu that it is in boot mode “flash/prom”, boot type is “intel hex

Browse for init file “\Analog Devices\VisualDSP 5.0\Blackfin\ldr\ezkitBF537_initcode.dxe”

And then rebuild project.

Then I programmed my new ldr file by Flash Programmer with default driver “\Analog Devices\VisualDSP 5.0\Blackfin\Examples\ADSP-BF537 EZ-Kit Lite\Flash ProgrammerBF537EzFlashDriver.dxe”

Programming & comparison was successful.

 

When I switched power off/on my application doesn’t start.

Boot mode of processor is set to “1” (BMODE pins is 001)

 

What I’ve missed trying to start my app from flash?

Is there a simple way to start VDK/LwIP based app from flash?

Outcomes