AnsweredAssumed Answered

Maximum Clocking of BF609 EvKit

Question asked by APlinge on Nov 8, 2012
Latest reply on Nov 19, 2012 by Prashant

Hello Everyone!

 

We started using an BF609EvKit for our Development, since we need a lot of processing power (up to 1000MIPS).

 

Surprisingly, when using the adi_pwr_GetSystemFreq function, it reported that the Cores are operating at 250MHz (10 x 25MHz CLKIN). We tried to increase the Core Clock using the corresponding adi_pwr_SetFreq functions, but although no error was reported, the Cores seems to run no faster than 250MHz... What am I missing?

 

Am I using adi_pwr wrong?

Is the BF609 already running 500MHz?

To what is Silicon Rev 0.0 actually limited?

 

Thanks,

 

Axel

Attachments

Outcomes