AnsweredAssumed Answered

ADV7181C in 625i 4x1 mode

Question asked by CRU on Nov 8, 2012
Latest reply on Nov 8, 2012 by DaveD

Hi,

 

I need to acquire RGsB PAL in 4x1 mode (54MHz sampling frequency and 720x576 output resolution).

My requirements are :

R on Ain5

G on Ain6 and SOG/SOY

B on Ain4

4:4:4 Output in DDR12bit with FVH syncs

 

I used adi scripts to begin and made some changes for my application.

 

The LLC clock frequency is 27 MHz instead of 13,5MHz and a pixel on two seems to be dark.

 

An idea ?

Regards.

 

My script :

{ 0x05, 0x00 },

{ 0x06, 0x0B },

{ 0xC3, 0x56 },

{ 0xC4, 0xB4 },

{ 0x1D, 0x47 },

{ 0x3A, 0x11 },

{ 0x3B, 0x81 },

{ 0x3C, 0x52 },

 

// Channel A / Y

{ 0x52, 0x00 },

{ 0x53, 0x00 },

{ 0x54, 0x07 },

{ 0x55, 0x0C },

{ 0x56, 0x94 },

{ 0x57, 0x89 },

{ 0x58, 0x48 },

// Channel B / Cr

{ 0x60, 0x08 },

{ 0x61, 0x00 },

{ 0x62, 0x20 },

{ 0x63, 0x03 },

{ 0x64, 0xA9 },

{ 0x65, 0x1A },

{ 0x66, 0xB8 },

// Channel C / Cb

{ 0x59, 0x08 },

{ 0x5A, 0x00 },

{ 0x5B, 0x7A },

{ 0x5C, 0xE1 },

{ 0x5D, 0x00 },

{ 0x5E, 0x19 },

{ 0x5F, 0x48 },

 

{ 0x6B, 0xC4 },

{ 0xC9, 0x08 },

{ 0x71, 0x20 },

{ 0x72, 0xD2 },

{ 0x7C, 0x00 },

{ 0x7B, 0x1C },

{ 0x8A, 0xB0 },

{ 0x85, 0x1B },

{ 0x8F, 0x77 },

{ 0x90, 0x29 },

{ 0xB7, 0x1B },

{ 0xBF, 0x06 },

{ 0xC0, 0x40 },

{ 0xC1, 0xF0 },

{ 0xC2, 0x80 },

{ 0xF4, 0x37 },

 

{ 0x0E, 0x80 },

{ 0x52, 0x46 },

{ 0x54, 0x00 },

{ 0x57, 0x01 },

{ 0xF6, 0x3B },

{ 0x0E, 0x00 },

Outcomes