AnsweredAssumed Answered

AD9959-How do you apply the AD9959 without using transfomers on DAC out?

Question asked by Mark-M on Nov 6, 2012
Latest reply on Nov 26, 2012 by DSB

I would like to use the AD9959 to produce freuqencies from 1Hz to 25MHz.  In order to go down to 1Hz frequency, a transformer can't be used on the DAC outputs.  How would one use the AD9959 DAC ouputs without a transformer?  Would one termnaite both to AVDD though 50 ohms, but only use oneof them going onto the AAF?  Could a resistive combiner be used to use both outputs?

Outcomes