AnsweredAssumed Answered

memory window: address x does not exist in the memory map

Question asked by pfeifferc on Oct 30, 2012
Latest reply on Nov 12, 2012 by CraigG

Hi !

i have following warning if i want to see the content of my external flash (start addr.  = 0x2000 0000)

"Warning: Address 0x20060000 does not exist in the memory map."

 

my XML init file (ADSP-BF537-proc) contains following adaptions to use our flash

<memory-segment start="0x20000000" end="0x200FFFFF" width="8" type="PM RAM EXTERNAL"     name="BLACKFIN Memory" memory-id="0" description="External Async Bank0 Memory"/>

 

whats wrong ? i use a custom board file - but on another installation of VDSP 5.0 B10 works with exact this files.

 

 

regards christoph

Outcomes