AnsweredAssumed Answered

AD 8223 for single ended operation.

Question asked by aydyjude on Oct 27, 2012
Latest reply on Oct 29, 2012 by aydyjude

I have to connect a  single ended low level signal(ac) to AD 8223's differential input. Can I connect AD 8223's -ve input directly to ground and the +ve input to the signal input with capacitor coupling for DC isolation? I have used 2.5V at the reference pin. The circuit is operating from single supply +5V and Gnd.

Outcomes