AnsweredAssumed Answered

questions about ADIS16360 Linux Driver

Question asked by ALCENGINEER on Oct 19, 2012
Latest reply on Oct 20, 2012 by NevadaMark

I am using the Linux Driver for the ADIS16360 ( actually for the ADIS16400).  Everything works Except fot the Reset. When I do a (cat Reset). I get a (cat: reset: Permission denied). I also tried it with a sudo. Any suggestions. The second is that I am on to writing the Algorithm.  But to do this I need a time stamp. I saw that there is a time stamp under the scan elements folder. However, there is nothing in the data sheet about it. If I can use the sensor timer that would be ideal. If not then I would have to use one of the clocks on the processor, which i don't believe would be as accurate. How is this usually accomplished?

Outcomes