AnsweredAssumed Answered

BF561: Triggering an interrupt in the other core

Question asked by Rai on Oct 16, 2012
Latest reply on Oct 16, 2012 by CraigG

Hi all,

I am using a "One application per core" type project in VDSP++, and I wish to have core A (producer) trigger an interrupt in core B (consumer) when new data is available. According to the hardware reference:

Signals can be passed between the two applications by triggering interrupts via the system interrupt controller. The run-time library allows interrupt handlers to be registered, but does not provide any direct support for the system interrupt controller or for raising events at that level.

How would one go about triggering such an interrupt (preferably in C)? Is there any example code available that does this?

 

Thanks in advance.

Outcomes