AnsweredAssumed Answered

AD5060 Eval LabVIEW driver not working.

Question asked by nicks on Oct 12, 2012
Latest reply on Oct 17, 2012 by musach

Hi,

 

I'm using the AD5060 Eval system and all works well when I use the supplied driver application, but when I switch to the LV driver I cannot get anything out of the device. The LV driver is not reporting any errors and it does find the board. I hooked up a logic analyzer to the 3 TP's on the eval board and can see the SPI transactions if I use the application but nothing if I use LV. I also want to drive the device with dynamic data... sine etc. rather than just set points hence wanting to use the LV driver. Has anyone seen this behavior from the LV driver and have they managed to get it working correctly?

 

Thanks,

 

Nick

Outcomes