AnsweredAssumed Answered

Reading problem in AD7294

Question asked by anoopgs@cdac.in on Sep 28, 2012
Latest reply on Oct 4, 2012 by jcolao

Hi all,

               I am working with AD7294  with frequency(SCL) 360 MHz.I had some problem with continues read .if i am giving some more delay between  two read it will be responding good,but if the delay is low it may work for two three read cycle and become hanged in read busy status .I cant get any idea from datasheet on the timing between consecutive reads.Is there any unknown spec.We have to get read operation quick.The device is taking around 100mA is it normal.So please give me some expert opinion or some one who could advice me.( found that its response is not proper if the time between two reads is less than 5 ms- not sure )

 

Regards

Anoop G S   

 

Message was edited by: Anoop GS

Outcomes