AnsweredAssumed Answered

AD607

Question asked by uWmaster on Sep 28, 2012
Latest reply on Sep 28, 2012 by jdobler

I have an AD607 demo board rev.C. I need an analog signal from AM demodulator from AD607.

My IF is 455kHz and I have connected DMIP and FDIN pins (1 & 15) together.

Is there anything else I must do around outputs or something entirely different,

than is not implemented on demo board, to achieve good amplitude demodulation? 

What is the max out level from demodulator? I would like to have audio signal as high as possible.

Outcomes